Rocol Flawfinder Cleaner Sprays is only available to buy in quantities of 1
Product Information
FLAWFINDER non-destructive inspection system is designed to provide a fast, reliable method for visual detection of cracks or flaws which would not normally be visible to the naked eye. Ideal for the inspection of welded joints, castings, forgings etc. FLAWFINDER Cleaner Spray is an aerosol applied cleaner used as part of the NDT crack detection system for pre-use cleaning. It can also be used for the easy removal of FLAWFINDER DYE PENETRANT and FLAWFINDER DEVELOPER Sprays. It is also an effective general purpose cleaner.