Knipex Pipe Cutters is only available to buy in quantities of 1
Product Information
Pipe cutter for composite pipes and protective tubes. The patented cutting mechanism operates with two guide plates. During cutting, these vertical plates run in the troughs of the protective pipes. Only the raised part of the protective pipes, the crest, is cut. With this system of cutting, the blade always remains at a distance to the inset pipe, so that protective pipes can be cut to size after they have been installed. A rotating movement at right angles to the protective pipe is used when cutting.