Enter replaceable head drill inserts, a breakthrough in high-performance drilling tools that combines precision and cost reductions, all while giving you a lot of adaptability in the process... Read more below.
Replaceable Head Drill Inserts Explored
Definition: Replaceable head drill inserts are the cutting parts that fit into replaceable head drill bodies. Consequently, these inserts are designed to be swapped out when they become dull or when a different size or type is needed - without replacing the whole drill. As a result, they are made from strong materials like carbide and are built to handle tough jobs and high speeds easily. The inserts are also very easy to attach and remove, making them very quick and cost-effective to maintain - or adjust the drill for different tasks. They are also often used in industries like manufacturing, where precise and efficient drilling is also required.
How to Choose The Correct Replaceable Head Drill Inserts for You?
Drilling is one of the essential machining processes across industries, but traditional solid carbide drills often wear out and require full replacement, driving up your costs and downtime.
Enter replaceable head drill inserts, a breakthrough in high-performance drilling tools that combines precision and cost reductions, all while giving you a lot of adaptability in the process.
With long tool life and replaceable cutting edges, they offer you significant advantages over traditional drill bits.
Consequently, we have put this guide together to explore everything about these inserts, from how they work to their applications and benefits, to allow you to work out how to choose the right one for you.
What Are Replaceable Head Drill Inserts?
Replaceable head drill inserts are precision cutting tools where the cutting head (insert) can be detached from the drill body or tool holder, allowing only the drill tip to be replaced once worn out.
As a result, these exchangeable head inserts are made from high-performance materials like carbide or cobalt, and therefore, ensure that you get a much higher cutting performance and longer tool life, all while reducing your tooling costs at the same time.
With a cylindrical shank and high-precision design, they are ideal for working with a variety of workpiece materials as a result.
Why Choose Replaceable Head Drill Inserts?
One of the primary reasons to choose replaceable head drill inserts is their cost-efficiency and the significant cost savings they can give you.
For instance as we covered above, instead of discarding the entire drill when the cutting edge dulls, you can simply change the exchangeable tip drill insert, which is more economical for you in the long run.
Types of Replaceable Head Drill Inserts
There are several types of replaceable head drill inserts; for instance, you have:
High-Performance Drills
These high-performance and high-productivity drill inserts are designed for more advanced industrial applications, as they can give you superior speed, high penetration rates, and an excellent surface finish.
These high-efficiency tools are ideal for machining difficult materials like cast iron, stainless steel, heat-resistant alloys, and aluminium alloys, to name a few.
Multi-Purpose Drills
Multi-purpose replaceable inserts can also handle a wide range of workpiece materials and drilling conditions, making them very suitable for workshops that deal with different substrates like aluminium alloys, brass, or mild steel, for example.
Consequently, these drilling tools, with exchangeable drill tips, give you a lot more flexibility and ease of use.
Materials Used in Replaceable Head Drill Inserts
Replaceable Head Drill Inserts can be made from many materials, such as for instance:
Carbide
Carbide is one of the most common materials used in replaceable inserts for carbide drills due to its hardness, high strength, and ability to retain a sharp cutting edge even at high temperatures.
This makes them ideal for high-speed drilling machines and machining heat-resistant alloys - all of which really contribute to long tool life and high-quality results as a result.
Cobalt
Cobalt drill inserts, part of the Cobalt & HSS drill bit category, are favoured in high-temperature applications due to their excellent heat resistance and toughness, especially when drilling hard alloys.
Consequently, these more high-performance drilling tools maintain sharp cutting edges even under intense conditions and are suitable for high-speed operations as a result.
High-Speed Steel (HSS)
High-speed steel (HSS), included in the Cobalt & HSS range, is another material used in some replaceable inserts, typically for cost-effective applications.
Though not as durable as carbide or cobalt, HSS provides you with sufficient wear resistance for many standard drilling operations, which in turn gives you many cost savings and reliable performance in inserting drill bits as well.
Coatings for Enhanced Performance
Advanced coatings like Titanium Nitride (TiN), Titanium Aluminium Nitride (TiAlN), or Diamond-like Carbon (DLC) can then be applied to inserts to help reduce friction even more, which in turn helps to improve their wear resistance and extend your tool life in more demanding conditions.
These coatings then can contribute to high-performance drilling tools with low cutting force, all while giving you efficient chip removal and a long tool life simultaneously - which, in turn, really does improve the efficiency of your cutting edges.
How Replaceable Head Drill Inserts Work
Replaceable head drill inserts also feature a precise, geometric design that allows them to be securely locked into the tool holder - or drill body - often featuring a cylindrical shank.
This robust connection between the main body and the insert ensures that you get minimal vibration when in use, all while improving your accuracy and tool life as well.
Some head systems can also incorporate internal cooling channels for efficient coolant delivery as well - which literally delivers coolant directly to the drill point, enhancing performance and tool longevity.
Working Mechanism of Indexable Inserts
The cutting edges of the indexable insert work with the workpiece material, removing material as the drill rotates.
As the cutting insert wears out, it can then be replaced without discarding the entire tool body - as in exchangeable tip drills.
Cutting Action and Chip Formation
These modern replaceable inserts can also feature optimised geometries at the drill point to produce smooth chips, helping you to achieve efficient chip evacuation and chip removal from the hole being drilled.
This design then reduces the risk of chip jamming, especially at greater drilling depths and hole diameters, as well - improving your hole quality and overall drilling efficiency in your hole-making applications as a result.
Applications of Replaceable Head Drill Inserts
Replaceable Head Drill Inserts have many application uses; for instance, these can include:
Aerospace Industry
In the aerospace industry, where high precision and consistency are really key, replaceable head inserts really do excel in drilling tough, heat-resistant alloys like Inconel and Titanium, for example.
As a result, these high-quality drilling tools provide you with the high levels of accuracy and high-strength performance needed for components like engine parts and airframes - operating effectively at high-speed machining conditions.
Automotive Manufacturing
Replaceable drill inserts are also widely used in the automotive industry for machining engine blocks, transmission components, and other precision parts.
Here, their ability to work with a wide range of workpiece materials, including steel, aluminium, and composites, makes these drilling tools ideal in this sector.
Mould and Die Machining
Mould and die production also often involves working with hardened steel.
As a result, replaceable head drill inserts with durable carbide cutting edges are perfect for creating high-quality moulds and dies without frequent tool replacement while they do so.
Energy Sector (Oil & Gas, Wind Power)
The energy sector also demands drilling tools that can withstand harsh environments, particularly in drilling operations for oil and gas.
Replaceable head inserts give the high strength needed for such challenging conditions, especially when dealing with great drilling depths and heat-resistant alloys.
How to Select the Right Replaceable Head Drill Insert For You?
Selecting the right replaceable head drill insert depends on various variables.
For instance, firstly, you should consider the workpiece material you are drilling — whether it's steel, aluminium, or a composite, which will influence your choice of insert grade and cutting insert material.
Also factors such as hole diameter, drilling depth, point angle, and overall length (Length L) also affect the insert selection as well.
High-speed and high-efficiency operations will also require specific inserts.
>
If you need help, our customer support is available to assist you in making the best choice as well.
Contact Customer Services
If you are still not sure which Replaceable Head Drill Inserts are right for you or you need help, then please contact our team, and we will be happy to help you understand which ones are perfect for you and your team.
Standard Delivery
We have also extended our ordering hours to offer you next working day delivery, making your shipping experience even easier.
Place your order online by 7 p.m. and choose the delivery option that suits you best to ensure the timely, hassle-free UK delivery of your products.
Standard next-day delivery is also available for all products ordered within the specified time, with free shipping for certain items as well.
Who Is MSC Direct?
Here at MSC Industrial Supply Co., we are a leading supplier of industrial tools, equipment, and maintenance supplies across the United Kingdom and can also offer you trade accounts.
We also serve a wide range of industries, from manufacturing and engineering to maintenance and beyond.
Consequently, our outstanding customer service and expert technical team, fast delivery times, and technical support make us a trusted partner for all your business needs as a result.