Beha-Amprobe Moisture Meters is only available to buy in quantities of 1
Product Information
Moisture meter MT-10 can be used to measure the amount of water in the wood or building material so that the woodworker can determine if it is suitable for the intended purpose. Building inspectors, carpenters, hobbyists and other woodworkers often are required to have moisture meters. Wood flooring installers, for example, have to verify that the moisture of the wood matches the relative humidity in the air of the building. If this step is skipped, a vast array of problems may present itself cracking, cupping, crowning, buckling, sunken joints and cracked finishes. Function includes Moisture meters for construction and timber, temperature measurement.