Starrett Tubular Inside Micrometers is only available to buy in quantities of 1
Product Information
The 124 solid rod inside micrometer set is the most popular inside micrometer because of their lightness, ease of use and range. It is very useful for measuring inside diameters of cylinders and rings and measuring parallel surfaces. The desired range is obtained by assembling rods and spacing collars to the micrometer head. Measuring rods are provided with a shoulder that is set accurately in the micrometer head and locked in position. When assembling rods to the A and B heads, the reading line on the micrometer head should be lined up with the marking on each rod. Each rod has individual length adjustment for the anvil by means of special wrenches furnished.